Questions fréquentes (FAQ)

Poser une question

Video: Presentation of the Schneider Electric Unica In-Wall Bluetooth Receiver



Enjoy your favorite music over superior speakers wirelessly with the Schneider Electric Bluetooth In Wall Bluetooth Receiver. The Unica in-wall Bluetooth receiver can be paired with any Bluetooth device such as tablets, laptops, mobile phones etc. Play music from any source on your device, like internet radio or streaming services such as Spotify or Deezer. You can also connect devices that don’t have Bluetooth using the AUDIO IN option. The receiver can be connected to two or more speakers of any model, type or brand.
Cela vous a-t-il aidé ?
Que pouvons-nous faire pour améliorer l'information ?