Schneider Electric France

Bienvenue sur notre site !

Choisir un autre pays

    • Default Alternative Text

      Large Enterprise Building Management

      Energy and operational efficiency solutions

    • The Edge, Amsterdam SmartStruxure dans le bâtiment le plus écologique au monde

      The Edge est une référence internationale pour l'environnement de bâtiment intelligent tout en mettant, en première ligne, le confort et le bien-être des occupants. Découvrez comment SmartStruxure™ aide à créer un environnement qui est efficace et inspirant.

    • Davis School District, Utah, US

      Public school district, with 90+ buildings covering nearly 10M ft2, transitions from legacy building management system to SmartStruxure™ solution in three hours. Results: increased operation and energy efficiency and a productive learning environment.

    • Sheraton on the Park, Sydney, Australia

      Luxury hotel improves energy efficiency with upgrade to SmartStruxure solution building management system and saves 15% in energy costs, enabling it to take advantage of AusIndustry’s Green Building Fund.

      Read Story
      Default Alternative Text
    • GwangHwaMun D-Tower, Seoul, Korea

      SmartStruxure solution delivers energy management and occupant comfort at ultra-modern, mixed use twin towers (commercial office and retail building) in the "heart of Korea."

      Read Story
      Default Alternative Text
      Personnes de différentes ethnies discutant du travail, de l'efficacité énergétique, du pétrole et du gaz

      Challenges

      Facing growing challenges, large enterprise building managers need a system to optimize energy consumption, maintain healthy and productive environments, and update aging facilities with anytime, anywhere access to information.
      Deux hommes examinant des données sur un écran, gestion de l'énergie

      Our enterprise control systems

      From a single building to enterprise facilities.

      Customer Value

      • Icône intégration Optimize building performance Gain significant financial savings during installation, operation and maintenance of your facility.
      • Icône Serrage de mains Maintain facility comfort and increase facility value Create a healthy, sustainable environment that increases occupant productivity.

      Facts

      • Icône énergie bleue 40% of the world’s energy is used in buildings.
      • Icône d'outils bleue 75% of a building costs over its lifetime will go to maintenance and operating expenses.
      • Texte alternatif par défaut Only 20% of facility managers use 80% of their BMS's available capabilities.
      • Icône EcoXpert bleue 30% of energy used in buildings is wasted because of inefficient BMS.
      • Icône bleue interactive By 2020, there will be 30 billion devices connected via the Internet of Things.
      • Default Alternative Text In developed economies, at least half of the buildings that will be in use in 2050 are already built.