Schneider Electric France

Bienvenue sur notre site !

Choisir un autre pays

    • Default Alternative Text

      Taking the field: Keeping the baseball legends one step ahead of the weather

    • Default Alternative Text

      Nous donnons le ton en matière d'innovation.

      Et ce, à tous les niveaux. Découvrez comment Schneider Electric se positionne en tant que leader dans le nouveau monde de l'énergie avec ses produits connectés, ses solutions et ses services.

      Regarder la vidéoVideo Découvrir nos solutions actuelles et à venir
      • We’re on the Red Sox team! Boston Red Sox Case Study

        Schneider Electric is right behind the Boston Red Sox. Our cloud services help them stay ahead of the weather. It’s a whole new ball game.

        • Red sox case study

        Texte alternatif par défaut

        The challenge

        As weather gets more volatile, businesses susceptible to extreme weather face increased risk.

        With 82 home games a year, the ground staff for the Boston Red Sox work hard to ensure that when the umpire shouts ‘Play Ball’, fans and players alike get the best experience possible.

        Since Fenway Park is an open air field, team officials need to keep a close eye on changing weather conditions. Lightning is real concern, as it can strike with lethal force out of the blue, up to 10 miles from the centre of a storm cell.

        That’s a risk David Mellor, Director of Grounds, isn’t willing to take. But with cancelled games meaning both higher costs and lost revenue, only one thing is worse than having to cancel a game for a storm. And that’s cancelling a game for a storm that never hits.

        redSox_02

        'The weather impacts how we staff and what jobs we do that day. It can even impact if a game’s being played.'
        -David Mellor (right), Director of Grounds for the Boston Red Sox

         
        The solution

        Improved weather forecasting with Schneider Electric WeatherSentry Services provides precision data about precipitation, wind, dew point, shade, heat, and lightning--all factors that impact how the players and coaches approach the game, and the safety of both players and fans.

        Accuracy is imperative. Bad forecasts affect performance and  results, which can cost the Red Sox millions of dollars.

        So the Red Sox rely on the consistency and reliability in data and consultations from WeatherSentry Services to assess weather conditions including the likelihood, severity, and timing of rain to optimize the home game experience for fans and minimize costs associated with delays or cancellations.

        Schneider Electric WeatherSentry Services with Lightning Manager helps sports organizations to implement best practices for turf lightning safety: monitor lightning in real time as it approaches as well as set up custom advisory and warning zones up to 60 miles from a location.


        WeatherSentry Services Fast Facts

        • The most accurate forecasting capability in the world
        • Independently ranked #1 in forecasting
        • Largest onsite commercial meteorologist team
        • Patented alerting capabilities
        • Experts on call to help with particularly tough calls

        redSox_06

        Now you can stay one step ahead of the weather with WeatherSentry Services

        Get a free trial

        Instantanés des projets

        • Texte alternatif par défaut Surveillez la météo
        • Texte alternatif par défaut Protégez le public et les joueurs
        • Texte alternatif par défaut Limitez les risques
        • Texte alternatif par défaut Gardez une longueur d’avance
        • Texte alternatif par défaut Prenez les bonnes décisions